Daikin Applied Enhances Self-Contained HVAC System to Support Building Decarbonization
Daikin News

Daikin Applied Enhances Self-Contained HVAC System to Support Building Decarbonization

Sep 1, 2026
New self-contained unit enhances indoor comfort and efficiency with low-GWP refrigerant R-32 and modular design

MINNEAPOLIS, Aug. 27, 2024

Daikin Applied today introduced the next generation of its self-contained HVAC system (Model SWP J-Vintage), a cost-effective, highly efficient unit enhanced with the low-global warming potential (GWP) R-32 refrigerant. Designed to meet the unique demands of floor-by-floor applications, the SWP J-Vintage offers a range of features and benefits to help customers reduce their carbon footprint while maintaining superior performance and low costs.

“The evolution of our self-contained system underscores Daikin Applied’s leadership in the industry’s transition to more sustainable HVAC solutions,” said Jim Macosko, vice president of product and sustainability solutions. The SWP J-Vintage sets a new standard for self-contained units, offering unparalleled efficiency and flexibility and solves critical installation and maintenance issues for building owners and facility managers.”

As customers look to decarbonize, the self-contained system is the first available with R-32, boasting greater efficiency and a low charge limit, ensuring safety in case of leakage. The unit offers a seamless transition for existing users of Daikin Applied’s self-contained systems, featuring familiar flexible MicroTech® controls and also incorporates a standardized ECM fan array for redundant operation, enhancing overall efficiency.

The SWP J-Vintage features a modular design that enhances its versatility and ease of installation, particularly beneficial in retrofit applications. The design allows for disassembly for easy transportation through standard 34-inch doorframes. The modular approach also supports efficient assembly on-site, optimizing space utilization and accommodating narrow hallways typical in commercial applications. By offering this flexibility, Daikin ensures that the system can seamlessly integrate into diverse building infrastructures, providing tailored HVAC solutions with minimal disruption to ongoing operations.

The self-contained unit meets the needs of two major vertical markets: residential high-rise buildings and mid-rise office-style buildings. With floor-by-floor usage capability allowing for 1-2 units per floor, the unit provides a distinct benefit for property managers and building owners looking to streamline installation and operation while maintaining high efficiency.

Daikin Applied is committed to leading the HVAC industry towards greater sustainability by prioritizing decarbonization and energy-efficient performance. The launch of the SWP J-Vintage is a testament to Daikin's ongoing efforts to decarbonize commercial buildings through the integration of advanced technologies and environmentally friendly refrigerants, aligning with Daikin's broader mission to build a resilient and sustainable future.

To learn more about Daikin Applied, and the full range of commercial and industrial HVAC equipment and solutions, visit www.daikinapplied.com. Also, follow the company on LinkedIn for the latest on HVAC technology, services and trends.

About Daikin Applied Americas 
Daikin Applied, a member of Daikin Industries, Ltd., designs and manufactures advanced commercial and industrial HVAC systems for customers around the world. The company’s technology and services play a vital role in creating comfortable, efficient and sustainable spaces to work and live — and in delivering quality air to workers, tenants and building owners. Daikin Applied solutions are sold through a global network of dedicated sales, service and parts offices. For more information or to locate a Daikin Applied representative, visit www.daikinapplied.com or call 800-432-1342.

 

#                 #                 #

Media Contact:
Aaron Parker
Communications Director
Daikin Applied
612-202-8774
aaron.parker@daikinapplied.com