Daikin Applied Adds Inverter Compressors to Rebel Applied Rooftop HVAC System
Daikin News
Energy Efficiency
Indoor Air Quality
Refrigerants
Product Launch

Daikin Applied Adds Inverter Compressors to Rebel Applied Rooftop HVAC System

Apr 11, 2021
Ultra-Configurable Unit Also Now Includes Precision. Temperature Control and Adaptive Refrigeration Technology

MINNEAPOLIS - April 11, 2021

Daikin Applied today announced updates to its Rebel Applied™ packaged rooftop HVAC system, known for its leading airflow and efficiency ratings, and compact footprint. Rebel Applied now comes with inverter scroll compressors, precision temperature and humidity control, and adaptive refrigeration technology, expanding its ability to provide unmatched energy efficiency and enhanced indoor comfort.

Driven by Daikin inverter technology, these new features boost Rebel Applied’s already best-in-class efficiency. Unlike staged compressors that operate at fixed points, the inverter technology modulates compressor and cooling capacity continuously from 100 percent down to 15 percent so the system dynamically responds to match the load of a building. This means constant temperature and humidity control, which helps reduce energy use and operating costs while enhancing occupant comfort.

By continually adjusting to building load, Rebel Applied consumes less energy at part load to deliver an Integrated Energy Efficiency Rating (IEER) as high as 20, more than 40 percent above the ASHRAE 90.1 Energy Standard for Buildings. In addition, engineers and building owners can select either a lead-circuit or dual-circuit inverter compressor configuration based on their efficiency targets and performance goals — an industry first.

“With accurate temperature and humidity control, Rebel Applied creates an ideal environment for occupants so they can operate at their most productive levels,” said Matthew Dodds, applied rooftop product manager, Daikin Applied Americas. “At the same time, facility managers can optimize energy consumption and provide bottom-line savings. Plus, the compact footprint and fully configurable cabinet makes Rebel Applied the right fit for every new construction or retrofit application.”

The addition of adaptive refrigerant control also allows Rebel Applied to intelligently manage refrigeration cycles to keep the system online and operating safely. On the hottest days or when loads are at their highest, the adaptive controls look at the entering and leaving refrigerant conditions, and modify the compressor and expansion valves to prevent overload and nuisance shutdowns. The supporting Microtech controller gives users the ability to monitor the system in real time as well, and regulate refrigeration performance to improve operation during extreme weather or occupancy events.

To complement the latest features, Rebel Applied is equipped with several indoor air quality (IAQ) technologies available as factory-installed options, including: UV lights to kill pathogens and prevent microbes from living in the unit, high-efficiency pre and final filtration to capture more contaminants, and humidifier grids that help produce ideal building environments.

“We’re in tune with buildings and indoor spaces more than ever,” Dodds said. “IAQ enhancements and precision controls that deliver quality air, and increase peace of mind and comfort are essential.”

Learn more about Rebel Applied, and follow Daikin Applied on LinkedIn for news and information on commercial HVAC equipment and services.

About Daikin Applied

Daikin Applied, a member of Daikin Industries, Ltd, designs and manufactures technologically advanced commercial HVAC systems for customers around the world. The company’s technology and services play a vital role in creating comfortable, efficient and sustainable spaces to work and live — and in delivering quality air to workers, tenants and building owners. Daikin Applied solutions are sold through a global network of dedicated sales, service and parts offices. For more information or to locate a Daikin Applied representative, visit www.daikinapplied.com or call 800-432-1342.

About Daikin Industries Ltd.

Daikin Industries, Ltd. is a Forbes 1000 global company with 2019 revenues of over $24.3 billion and more than 70,000 employees worldwide, making it the largest HVAC manufacturer in the world. Daikin is engaged primarily in the development, manufacture, sales and aftermarket support of heating, ventilation, air conditioning and refrigeration (HVACR) equipment, refrigerants and other chemicals, as well as oil hydraulic products. Daikin was named one of the world's most innovative companies by Forbes magazine. For more information, visit www.daikin.com.

# # #

Media Contact:
Aaron Parker
Director of Communications, Daikin Applied
612-202-8774
Aaron.Parker@daikinapplied.com